The effectiveness review verifies that the completed actions actually resolved the original problem without creating any additional problems. The Follow-up Auditor/Reviewer selects an Effectiveness Auditor/Reviewer.
The team members determine how the effectiveness of the corrective action can be tested or measured. The Effectiveness Auditor/Reviewer checks for proof that the problem is prevented and there is no chance of another occurrence of the same event. If the problem is serious or there is not complete control over corrective action implementation, periodic effectiveness checks are required.
The following table provides the fields available under Auditor/Reviewer Information section:
Field |
Description |
Auditor (Reviewer) |
The auditor/reviewer is responsible for verification of corrective action effectively.
|
Scheduled Date |
The scheduled date is the date that the audit/review was scheduled.
To choose the Date/Time to Owner date:
OR
|
Actual Date |
The actual date is the date that the audit/review was conducted.
To choose the Date/Time to Owner date:
OR
|
Remarks |
The auditor/reviewer enters any remarks about the audit/review conducted. |
The Disposition section provides the final determination of the effectiveness auditor/reviewer. The effectiveness auditor/reviewer selects the “Accepted” check box if the audit evidence is sufficient, or rejects if the corrective action is not effective. The auditor/reviewer issues a new CAR if new events are found where corrective actions need to be implemented.
Field |
Description |
Name |
The name of the effectiveness auditor/reviewer is automatically populated when the auditor/reviewer marks the disposition as Accepted or Rejected by selecting the respective check boxes. |
Date |
The date and time of the disposition. This field is populated when the corrective action is saved. |
Accepted |
The effectiveness auditor/reviewer selects the Accepted check box, if there is evidence that the corrective action is effective over a period of time. |
Create New CAR |
To close the current CAR and open a new CAR with a sequential dash number:
|
New CAR |
|
Rejected |
The effectiveness auditor/reviewer selects the Rejected check box, if:
|