To Specify the Filter Conditions:
Select the AND / OR logical condition from the drop-down menu.
Select the field from the drop-down menu.
Choose the type of comparison from the drop-down box (equals, greater than, and so on).
Enter the value of the selected field in Step 2. The value is required to be a valid choice for the field in step 2.
Click Add.
To select the fields to be displayed in the customized report, see Field Selection.
For more information about the fields in this screen, click here.
|
Field |
Description |
|
|
Select the condition AND / OR from the drop-down menu. |
|
|
The field choices include CAR ID, CAR Status, Owner Name, and so on. Select the field name from the drop-down menu. |
|
|
Select one of the conditions from the drop-down menu. The conditions in the drop-down menu are:
|
|
|
Enter the value of the field name. For example, if the selected field name is CAR TYPE, the value of the field can be Internal. |
|
Add |
To add the filter to the list box, Add. |
|
Clear |
|
|
Clear All |
To clear all of the filters in the text box, click Clear All. |
Note
Multiple filter conditions may be added to the report.
If no fields are selected in the Field Selection tab before clicking Accept, a pop-up opens.